This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A49: datasheet possible error.

Part Number: TPS7A49

Looking through the datasheet for the TPS7A49 and looking at the typical application example.  Specifically page 17.  Equation 5 calculation of R1.  The calculations comes out to 1.265K.  However, the next line says to select R1 at a value of 68.1K.

Is this an error in the datasheet?

  • Hi Greg, 

    Thanks for the feedback. You are correct, the values of R1 should be 1.25K Ohms not 68.1 KOhms. The 68.1KOhms will generate a 2V output instead of 1.2V. This error will be fixed next time when we release a new revision of the datasheet. 

    Regards, 
    Jason Song