Hello
We are using the TPS61030 with two large super capacitors (60F each tow in series) the capacitors when charged can be at voltages as high as 5V. The super capacitors are very low internal impedance capacitors (<20mOhm) and are capable to very quick rise times.
We have observed that when these capacitors are hot plugged to the TPS61030, the device fails and stops functioning, even after disconnecting the capacitors, power cycling etc. It is permanent failure of the device.
Is this expected behavior, if so is there a recommended work around to this problem.
Thanks
DG