Hi team,
I have some questions about TPS2549IRTERQ1
1. How does hysteresis work in DP_IN and DM_IN SHORT-TO-VBUS PROTECTION? If the protection is triggered at 3.7V, then it will be released at 3.6V with 100mV hysteresis?
2. Are DP_IN , DM_IN and DP_OUT,DM_OUT pins powered with different supplies? Or they are connected directly? I see the switch on resistance of DM and DP is around 2 ohms, will the voltage of DP_OUT,DM_OUT pins be lower than DP_IN , DM_IN because of the voltage drop on the switch resistor?