This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM84209: Layout Recommendation for Switch Node

Part Number: TPSM84209


Hello,

In the Pin Function table of the datasheet it recommends the following for the SW (switch node) pins:  These pins are connected to the input side of the internal output inductor. Do not place any external components on these pins or tie them to a pin of another function.

But in the layout the pins are tied together with a small pour. So while the note doesn’t tell you to tie them together, the layout example is not going against the pin function table's recommendation. My customer is asking if it is recommended to tie the nets together like the layout picture (Fuigure 34) in datasheet. It looks like a good idea but I wanted to get confirmation from you all.

Thanks and happy holidays!

John