Hello,
My customer is interested in UCC28881 and have a question.
According to Figure 17 on the datasheet(SLUSC36B), the output voltage increase at the light load and this graph shows 12V output case.
They would like to know 5V output case. Do you have the same graph for 5V output case?
And 9.2.1.2.7 explains this no-load regulation performance highly depends on the time constant configuration.
Do you have any data about how much regulation performance can be realized at 5V output case?
They want to connect a LDO to this UCC28881 output and they have to know the max input voltage of this LDO.
Regards,
Oba