This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24040: bq24040

Part Number: BQ24040


Hi Sir,

In normal 5V input condition, /CHG pin shows OPEN when battery full charge.

Will /CHG pin also shows OPEN in below condition?

1. OUT Short-Circuit Protection?

2. ISET Short Detection?

3. Overtemperature Sensing Protection?

Thanks, Ian.

  • Hi Ian

    See below.

    "Will /CHG pin also shows OPEN in below condition?"

    1. OUT Short-Circuit Protection? -- Bill J - /CHG Open

    2. ISET Short Detection? -- Bill J - /CHG Open

    3. Overtemperature Sensing Protection? -- Bill J - For TS pin low  /CHG Open