Questions:
1. If the battery is reversed, there is nothing in the TPS1HB16AQPWPRQ1 to prevent reverse current. Section 9.3.1.4 suggests using reverse blocking FET or Diode, which to an extent defeats the purpose of using the TPS1HB16AQPWPRQ1. Are there any parts similar to TPS1HB16AQPWPRQ1 (size, cost) that don't allow reverse current? If not, is there a recommended FET, and is there an application circuit?
2. During startup, there will be inrush current to charge capacitors. Will the current limit turn off the TPS1HB16AQPWPRQ1?