This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: Need clarification on peripherals around DSG mosfet circuit

Part Number: BQ76952

Dear TI Team,

As given in the sample schematics in datasheet and evaluation board's manual, could you please clarify the role of circuitry involving Q4, R33, R35, D8, R40 and D10?

Regards 

Manuj

  • Hi Manuj,

    The components in question are for reverse charger protection.  DSG does not go below VSS, so without the clamp circuit of Q4 the gate of Q3 would remain near 0V and Q3 would operate in a source follower mode while a reverse charger was attached.  With Q4 on Vgs of Q3 is about 0, Q3 remains off and PACK+ falls to a negative voltage.  This creates a large voltage across R39 and R41 which are sized to dissipate the power required in that condition.  Since R39 and R41 are a large value to keep the power dissipation manageable, turn off would be slow, so D10 and R40 operate in parallel for DSG turn off to turn off the Q3 in a suitable time. 

    See the application note https://www.ti.com/lit/pdf/sluaa09 section 2 for test result and additional description.