This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LED driver to drive 8.5V 100mA UVC LED

Other Parts Discussed in Thread: TPS61169, LM3697, LM3509

Hi support :

I have a new project.
The LED is UVC LED.
The attached file is the I-V curve of the LED.
The Vf is very high.
Please help to advise good solution to drive LED.
I wish to have I2C or SPI or other serial interface for MCU
to control the LED driver.
The brightness controll could not be the PWM.
I need to drive the LED in different LED current.
I need to sink the LED in different current.
I wish to have 32 or higher brightness steps.
Please help to advise good solution.
Thanks.