Part Number: TPS2595
Hello,
My customer has a question about the TPS259541 design.
Could you please tell us the reson why SMBJ16A-13-F TVS was selected for the TPS2595EVM input stage?
The max clamping voltage of the SMBJ16A is 26V. But, the absolute maximum input voltage of the TPS2595xx is 20V.
If a voltage higher than 20V is input, will the TPS2595xx not be damaged?
Is SMBJ12A(V_RWM:12V, Max Clamping Voltage: 19.9V) suitable for VIN, VOUT 12V ?
Thank you.
JH