Other Parts Discussed in Thread: GPCCHEM, BQ34Z100
Hello,
I have a problem regarding the BQ34z100-G1 Fuel Gauge Device.
I am not able to successfully complete a learning cycle.
The learned status stays 0x04, even when correctly following the SLUA903 document.
I was able to use this device correctly in the past, however that was using a Nickel based chemistry.
Currently I am using a 30Ah 6S Li-Po based battery, but it is advertised as a solid state Li-Ion.
I ran a GPCCHEM cycle, which correctly returned multiple suggested usable chemistries.
However, using both the recommended chemistry (0x0508) as the secondary chemistry (0x2588), I am not able to complete the learning cycle.
The pack is sufficiently rested as shown by the OCVTAKEN, RUP_DIS and VOK, The FC bit gets set, but still the learned status won't increase from 0x04.
I've included a log of a dsg-rel-chg-rel-dsg cycle, which may provide some insight into the issue that I am experiencing.
Also included in the file are the results of the GPCCHEM tool.
Before the log cycle, I did forget to set the scaled bit but this shouldn't effect the operation of the device.
I'm using a scaling factor of 7.0, also applied to the configuration and gas gauging parameters.
This file is also included.
If you are able to provide me with any clue of what i'm doing wrong, it would be perfect!
(Side note, I've tried 5 failed cycles with the 0x0508 chemistry, and 1 with the 0x2588, which didn't help. Also tried modifying taper current, which either resulted in no FC detection, or same learning status as 0x04)
Thanks in advance!
Thierry