Hi Sir/madam,
the requirements for which chip has been designed is
i/p :15V/2.5A
o/p: 12V/1.2A
only battery without system
i am getting output voltage at the battery terminal like 10.6 V and system voltage it is showing as 13.44v for me i need to just charge the battery of 3s configuration and battprez everything is proper and i doubt that it is charging my battery also so please help me these
thank you