I know the BQ24721-G1B supports a Current Deadband threshold; Average Current will report 0 for any average currents that are below this threshold. I also know that some of your fuel guages also support a Coulomb Counter Deadband, which is used to exclude current measurements that fall below this threshold for inclusion in coulomb counting. Questions:
- Does the BQ24721-G1B have a configurable Coulomb Counter Deadband? I don't see one listed in the Technical Reference.
- If not, does the BQ24721-G1B have a hardcoded Coulomb Counter Deadband? And, if so, what is it?
- If not, given the integrated 7 mΩ sense resistor, what is the minimum current that can be counted by the BQ24721-G1B Coulomb Counter via the integrating ADC?