The datasheet (section 10.2.2.5) for LMQ61460-Q1 states that the minimum input capacitance is 10uF. Questions:
1. The users guide (SNVU698A) shows 2 x 4.7uF ceramic capacitors, UMK325B7475MMHT. This capacitor does not have a capacitance vs. voltage spec, but similar capacitors show a 30-40% drop in capacitance at 24V. Will 2x4.7uF work at 24V and higher?
2. Can I use a single 4.7uF ceramic capacitor in parallel with a 100uF electrolytic capacitor (EEH-ZA1H101P)?
3. Currently the LMQ61460AASQRJRRQ1 is only available from TI. When will it be available at distributors?