This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27520-G4: bq27520 FC Jump to 0 after 1 hour of full charge

Part Number: BQ27520-G4

Hi

My customer use BQ27520-G4,and also finish CHEM-ID and Cycle Learning. They found that the battery is full charged and [FC] bit was set to 1,  after about 1h, the [FC] bit will jump to 0 again. The following is the log file. From the log file, State Of Chg is always 100%. Why does the [FC]bit jump?

bq27520 (2).log

Thanks

Star