This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24650: Battery Management Solution for Small home appliances

Part Number: BQ24650
Other Parts Discussed in Thread: BQ77915, TIDA-050042

Hi Team,

This is customer request can you please advise with which combination you recommend:

"

We aim to design a charging circuit with a lithium-ion battery.
We can use 6 or 7 serial 18650 2000-2500 mah batteries in total. Accordingly, we should design a charging circuit that includes current protection and balancing features. During charging, the cell is usually charged with 30-35% of its current. The charging circuit must be able to meet this current. We need to provide a charge current up to max 1A.

"

Our initial idea is BQ77915 + BQ24650, what do you think?

Thanks in advance

Best Regards

Furkan Sefiloglu