This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54302: SW waveform is oscillated.

Part Number: TPS54302
Other Parts Discussed in Thread: TPS54308

Hello ~
I have a question on TPS54302. The question is as below description,

Application information,
1).Vin=24V, Vout=5.0V
2).Iout=1.8A(typ.)

Q1:The SW pin output waveform is not quite as a square wave. It is disturbed. Especially on 500mA and 1.5A which compare with TPS54302 datasheet(Fig.23).

Q2:In the Iout=3.0A, Why does the high side SW width is not the same ?

I provide 4 conditions which are Iout=100 mA, 500 mA, 1.5A and 3.0A. Please refer attached file and let me know your opinions. Thank you in advance.TPS54302 SW waveform.pdf