Related to https://e2e.ti.com/support/power-management/f/196/p/959057/3543576
I need charger detection via USB data pins. However the same USB pins are used by the CPU. CPU can be unpowered so the USB pins need to be muxed.
I added a USB2.0 HS compatible mux.USB data pins are connected to the charger IC by default. I need to control the MUX to connect data pins to CPU after BQ25790 USB host/charging port detection is ready.
Is PG signal related to USB host/charging port detection or is it voltage detection only?
The answer to my preivous question says BQ25790 needs 2s max. for detection. I could use some kind of timer circuit but it would be better if PG or some other signal can be used from BQ25790 IC.