This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28782: Minimum and Maximum Switching Frequency

Part Number: UCC28782

Hello Guys,

What is the minimum to maximum switching frequency of UCC28782? it' doesn't seem to be described in the datasheet.

Thanks in advance!

Art

  • Hi Art,

    UCC28782 is not a fixed frequency controller, It operates at transition mode.  The minimum switching frequency happens at lowest input voltage and full load. since the controller has burst mode controller . the maximum frequency happens at minimum Vcst threshold ~0.15V . In a word , the switching frequency is decided by bulk voltage , transformer inductance and output load condition. the switching frequency can be changed by adjusting transformer inductance .

    Thanks.