This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM3464A: LM3464A

Part Number: LM3464A
Other Parts Discussed in Thread: UCC28740, LM3464

Tool/software: WEBENCH® Design Tools

To whom it may concern, I am using the LM3464A LED driver to power a series of LED. I am utilizing all 4 output of the driver. I am trying to design a power supply using the webench software that can handle my requirments. I have a forward voltage for the series LED (1 out of the 4 channels) that has a forward voltage of 64 volts. The average LED operating current is 700mA. I have attached the power supply that was generated in WEBENCH. Will this work with the driver for all 4 channels or is the power supply output current to small? Does the power supply output current have to be 700mA x 4 = 2.8A at minimum to drive all four channels each at 700mA?Draft1_PowerSupply.pdf