This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS82130: TPS82130 Specifications

Part Number: TPS82130


We need to know below specification of TPS82130 for the specified input & output requirements. Seen the similar query in some other thread, but further discussion was in private mode. 

Two combinations are required: One 12V to 5V and second 3.3V to 1.2V

Vin=12V / 3.3V

   Vout=5V / 1.2V

   Iout=1.5A / 0.5A

   Thermal Derating

   Load Regulation

   Line Regulation

   Switching Frequency

   Input and Output Ripple in PWM Mode

   Input and Output Ripple in PSM Mode

   Load Transient

   Startup without Load

   Startup / Shutdown with Resistance Load

Regards

Hafiz