We are planning to start developing a new retrofit BMS kit for drone flight batteries based on LiPos. The kit should be modular, that means a base board with the bq40z80 ic, a LED with push button board, a shunt board and a FET board. This to accomplish various application requirements ranging from simple cell monitoring without columb counting and protections to full features including protections.
flight batteries usually don’t want to have discharge FET protections as this will terminate the flight and to crash the drone. However, the pre-discharge FET will be a good feature to avoid sparks in the connectors as the load are motors with ESC with high capacitors.
will it be possible to use the pre-discharge FET only?
will be a modular design based on more boards be a viable solution?
we also handle high current up to 150 Amps. Is there any reference design to use a current hall sensor connected to the shunt pins using a resitor voltage divider?
I have more questions, but would like to go through it step by step.
Thanks,
Jarno