Other Parts Discussed in Thread: BQ27427, TIDA-01012, EV2400
Hi,
I've couple of questions for the fuel gauge: BQ27426
We are using BQ27426 and info from the application example (page 18, document date: SLUUBBO-December 2015) is not quite clear. In the document, page 35 (data flash summary table) Offset for design capacity is 6, design energy is 8 , termination voltage is 10 and taper-rate is 21; all numbers are in decimal. However I'm not clear how the application example (page-18) concludes the offset is 0x4A for design capacity instead of 0x46? Which one is correct - 0x4A or 0x46?
On our board, we don't use BIE auto detect; We have gauge's BIN pin and charger's TS pin shorted to Vss with a 10K pulldown. In order to store the design capacity info and successfully use the fuel gauge should we clear the BIE setting to 0 in bit-5 (OpConfig - Register) from the default setting of "1" before we store design capacity and other info? Should we use BAT_INSERT command before we start storing new design capacity info? If not then at what sequence we need to issue BAT_INSERT command? Do we need to update the checksum of OpConfig register if we clear the BIE bit?
In order to change Chem-ID to 1202 do we need to write 0x01 or 0x00 to the Chem-ID register 0x0031?
Instead of writing various data to the gauge programmatically in steps is it possible to update gauge's flash memory in one go with all the changes? Where can I find info on how to update flash memory altogether?
Thank you for helping,
- Andy