This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TPS53315: ripple injection circuit

Part Number: TPS53315


Tool/software: WEBENCH® Design Tools

hi,

i have shared my WEBENCH design below

https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=8E9069BE200976FA  

OUTPUT -5V , INPUT -12V, OUTPUT CURRENT -11A, FSW 500KHz

in my ckt 

L1- XAL7070-182MEB (SAME)

Cout   ( Ceramic cap) : -   100uF  16V 1210 20 % X5R( qty 4) 

                                           47uF  16V 1206 20 % X5R( qty 4)

 Total de-rated capacitance :- approximately 287uF 

could you please check the ripple injection and feedback network is okay?

In the datasheet less than 50mV target is mentioned for VINJ_SW, but there is no recommendation for VINJ_OUT.

is there any limit consideration for VINJ_OUT.?

And also while Calculating VINJ_OUT should we need to use de-rated Cout value or total Cout?

could please verify Rr, cr, Cac, Rfbt & Rfbb values are okay or need any fine tuning?

thanks and regards

Adarsha A N