Part Number: BQ2980
Hello,
i am currently using the BQ298010 as a protector for my LiIon charging board.
Everything is working as expected except from the CTR Pin function: I am able to trigger the Reset-Function by pulling the CTR Pin high to 3.3V. But I am not able to trigger the Shutdown-function, because the System resets itself after applying 3.3V on CTR pin for >5.4 seconds, as mentioned in the datasheet.
I am expecting to use the Shutdown-function to conserve Battery. I then want to wake the device up again by applying a charging Voltage like it's the case when the BQ2980 enters Shutdown-mode because of UVP.
I will attach the schematics of my charging circuit.
Kind regards
Björn Ellensohn