This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28070: How to improve current distortion and harmonics

Part Number: UCC28070


Dear Ti community

I'm developing PFC by using this IC.

But there are some problems.

The result of the  harmonic measurement is bad.

when middle ~high load, beyond the IEC standard.

I attach  waveform by  oscilloscope.

Yellow is input voltage,red is input current.

I attach my design too.

When there is other necessary information for a solution, please reply.

Please tell me a  improvement plan.

6153.TI.zip

  • Hi, 

    First of all, The calculator cannot be opened. 

    here is the improvement method of THD:

    1. Increase Dmax to 0.95

    2. the resistor divider on VINAC and VSENSE pin should be same.

    3. The capacitor on VINAC pin should be close to VINAC pin.

    Another tip: use very stable AC source as input. 

    Regards,

    Yunsheng