Other Parts Discussed in Thread: UCC28063A, UCC3895
Hello,
I am looking for some support on synchronizing this part to a downstream PWM converter.
Please advise.
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi David:
there is no a pin special designed or showed PFC ok signal for downstream PWM controller, I would suggest you can add external circuit by sampling PFC bus voltage through Vsense pin and compare with a reference votlage with a comparator or amplifier to get the PFC OK signal for downstream PWM controller.
UCC28063A has a pin"PWMCTRL" that designed for downstream PWM. You can use the same idea for UC3854.
Hope this helps you.
I am not looking for a PFC ok signal. I am looking to synchronize the oscillator to an external clock. Please advise.
Yes, please advise ASAP. I did find application note Slua245.
On another note, I need to synchronize three UCC3895's to an external clock. I see it has a bidirectional SYNC pin.
The data sheet is very limited on how to connect this pin to other UCC3895 ICs. Please provide any additional information.
Thanks
Hello David,
it is a pity that you are not satisfy with the E2E support. in order to have a good communication on the post, you also need to respine to the post ASAP.
can I know whether SLUA245 answers your question?
For UC3895, I would suggest you can refer the SLUA609 as a reference.
I would also suggest you can create a new post for UC3895 if you still have a question.
The E2E needs to cover a device in one post.
.