Hi,
I am trying to find a low power supervisor IC which can monitor the frequency change and give an alert to the Microcontroller when the frequency is out of the programmed threshold (i2c, .etc).
I investigated some supervisor & reset ICs like "TPS3430: Programmable Window Watchdog Timer ", and some counter IC, and also some ADC like ADS111x-Q1, but both of them can not completely fulfill my requirement.
I am planning to develop a wireless anemometer with the battery as the power supply, to get the long battery life, I need to detect the wind speed change (vane rotation speed change, frequency change) and use it to wake up the whole system to do the wind speed measurement. The wind speed change in electrical is a frequency change, when the system read the current frequency, the wind speed can be calculated, at the same time a threshold can be set via i2c bus to the monitor according to the current frequency, to allow the system wake up next time when the frequency is out of the threshold.
Please give me some suggestions, thanks.