Part Number: TPS51206
Hi All,
I have a question about TPS51206.
The sequence in 7.3.6 is as follows.
Turn on VDD, S3, S5-> Turn on VLDOIN and VDDQSNS
The sequence in Figure 23 is as follows.
ON-> ON VLDOIN and VDDQ SNS-> ON S3, S5
I will think both sequences is normal operating.
Which is the reference sequence?
Also, if VDD, VLDOIN, S5, S3 is Off, input 1.5V to VDDQSNS.
Does this condition result in malfunction or failure of the device?
Best Regards,
Ishiwata