This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65381A-Q1: Enable the ENDRV pin when debugger is connected.

Part Number: TPS65381A-Q1

Hi,

we are using TPS65381A-Q1 with renesas controller and the device is intialized with all proper settings and watchdog mechanism and we could see ENDRV pin is enabled by TPS65381A-Q1(through scope it is 5v continuosly).we want to see the same when debugger is connected(TPS65381A is always in safe state(4) not in active state(5)).we do not have bootloader at the moment in our project.

- Since it is working very well without debugger ,can we exclude some initializations/or some forceful methods to make ENDRV(pin32) output as HIGH from TPS65381A when debugger is connected.

Thanks,

P Tulasi Krishna.