Part Number: TPS56528
Hello TI experts,
my customer is designing a PCB with TPS56528. they used 2 ICs in PCB.
the problem is, one IC is working well and have no problem. but another ic have too high temperature when working.
here is the IR camera screenshot with 25℃ room temperature.
the left TPS56528 is 51.2℃, and right one is 66℃.
and in real situation, the temperature of IC top is 90.9℃ with 60℃ ambient temperature.
here is the schematics and layout of 2 ICs.
1) IC with no problem, Vout=0.8V
2) IC with heat problem, Vout=1.0V
3) and here is the current waveform of 12V input and 1.0V output.
please check this issue, and if there are any points for improving this heat problem, please let me know. Thanks.
Best regards,
Chase