Did a qualified discharge and logged it, see attached.
During the discharge, batt stat remained at 0x4125. The second to last row this changed to 0x0081, and the last row was 0x0001. In this last row, the column FullChgCap changed from 2200 to 9900, which is very close to design capacity and is correct. However, this was NOT saved into the gauge. A few rows later after power cycling the gauge, FCC remained at 2200.
1. How do I get FCC to save?
2. How do I get SOH to update? It remains at 22% too.
For convenience I attached the log file as both TXT format and XLS format.resistorTest2roomtemp_highrate.log.xlsx