Other Parts Discussed in Thread: GPCCEDV,
Hello,
I submitted the 6 battery test data logs to the TI calculator and got the CEDV parameters listed below. I loaded them into the gauge, charged a battery, and then discharged it. However, It shows SOH = 22% and the state of charge is incorrect. Gauge got to 0% SOC at 2080 seconds (Vstack = 12.712V) but the battery didn't finish discharging until 9028 seconds (Vstack = 10.272V).
Attached is the gg file and the log.
Battery Discharge Test 20201229.xlsxsm_bq34110Settings20201229.gg.csv
EMF 3083
EDVC0 58
EDVC1 0
EDVR1 198
EDVR0 243
EDVT0 3836
EDVTC 9
VOC75 13273
VOC50 13164
VOC25 12966