This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS735: Recommended value of feedback resistor

Part Number: TPS735

Hello team,

I would like to ask a question about the feedback resistor of TPS73501.

In datasheet, "6.3 Recommended Operating Conditions", 110kOhm is recommended for feedback resistor R2.

But in the other thread, there was a description that "noise will be optimized at R1||R2 = 250 kOhm". (This value 250kOhm also appears on the datasheet 8.2.1.2.)

Is there a reason why the recommended resistance value for R2 is 110kOhm? Which should be prioritized when determining the resistance value?

E2E thread | TPS73501 minimum value of feedback resistors(https://e2e.ti.com/support/power-management/f/196/t/519228)

Best Regards,

Ryotaro Fukui