With BQ24261M, the WARM and COOL thresholds are not independently programmable. The COOL and WARM NTC resistances for a selected resistor divider are calculated.
Is the HOT Temperature programable or changeable or is it fixed at 60 degrees C? based on the fact that RHOT (the NTC resistance at the hot temperature) is used as an input to determine RCOOL and RWARM.