As the title suggests, I'd like some clarification regarding the EN pin of the LM3409. I'm using the IC for a constant current source that needs to be selectively enabled/disabled via a digital pin from a microcontroller. If I drive the EN pin low, will this also turn off the PFET? The load and supply will remain connected to the circuit at all times. Is the LM3409 capable of disconnecting the load from the supply on its own or will I need additional circuitry?
Thanks,
Brian