This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: Alert pin not asserting after initial

Part Number: BQ34Z100-G1


Hello;

I've configured the Alert pin to assert on several events, including FC. But when the FC flag is raised, no interrupt occurs. However, if the capacity is low, I get an initial interrupt during device initialization, but thereafter, no ISR fires, despite the FC flag (as well as any others) being asserted. It seems as if the gauge requires the host to reset these flags, just as on the 34z110 and 78350 gauges.

Will you please confirm that the gauge does NOT require an Alert reset command, and if not, why is it not asserting the Alert pin when FC is asserted?

AlertCfg.docx

  • Hi Jeffrey,

    Could you share a log of the test so we can see the registers along with the .gg

    Thanks,

  • I cannot run my application and studio concurrently, and so these files are exported when the application is paused. Note again that the FC bit is set, but it does not assert the Alert pin. That makes me suspicious that the 34z100  requires a reset of the ALert, just as its sister gauge the 34110.Studio.gg.csv

    Wed Jan 06 09:17:48 EST 2021
    
    Device Version Info = 0100_0_16
    BQZ Device Name = bq34z100G1
    BQZ Firmware Version = 0_16
    
    
    Sample,DateTime,ElapsedTime,Control,CtrlStatus,StateofCharge,MaxError,RemCap,FullChgCap,Voltage,Current,AvgCurrent,Temperature,AverageTimeToEmpty,AverageTimeToFull,AvailableEnergy,AveragePower,InternalTemperature,CycleCnt,StateofHealth,ChargeVoltage,ChargeCurrent,PackConfig,Flags,Flags B,GridNumber,LearnedStatus,DoDatEOC,Qstart,TrueRC,TrueFCC,StateTime,DOD0PassedQ,DOD0Time,DOD0,QmaxDOD0,QmaxPassedQ,QmaxTime,LogRowTime(ms),LogStatus
    1,2021-01-06 09:17:53,4.000,0x0016,0x0004,100,100,23,23,25096,-2318,-2314,35.2,1,65535,7,-727,7.0,0,1,28800,1709,0xF8E7,0x0217,0x0400,12,0,16081,23,277,23,107,-318,2,16384,0,-319,2,934,SUCCESS
    2,2021-01-06 09:17:59,10.962,0x0016,0x0004,100,100,23,23,25096,-2317,-2315,35.2,1,65535,7,-727,7.0,0,1,28800,1709,0xF8E7,0x0217,0x0400,12,0,16081,23,272,23,114,-313,2,16384,0,-314,2,927,SUCCESS
    3,2021-01-06 09:18:02,13.566,0x0016,0x0004,100,100,23,23,25096,-2317,-2315,35.2,1,65535,7,-727,7.0,0,1,28800,1709,0xF8E7,0x0217,0x0400,12,0,16081,23,271,23,116,-312,2,16384,0,-313,2,935,SUCCESS
    4,2021-01-06 09:18:05,16.144,0x0016,0x0004,100,100,23,23,25096,-2318,-2316,35.2,1,65535,7,-727,7.0,0,1,28800,1709,0xF8E7,0x0217,0x0400,12,0,16081,23,269,23,119,-310,2,16384,0,-311,2,933,SUCCESS
    5,2021-01-06 09:18:09,20.002,0x0016,0x0004,100,100,23,23,25096,-2317,-2316,35.2,1,65535,7,-726,7.0,0,1,28800,1709,0xF8E7,0x0217,0x0400,12,0,16081,23,266,23,123,-307,2,16384,0,-308,2,936,SUCCESS
    6,2021-01-06 09:18:13,24.003,0x0016,0x0004,100,100,23,23,25096,-2315,-2316,35.2,1,65535,7,-727,7.0,0,1,28800,1709,0xF8E7,0x0217,0x0400,12,0,16081,23,264,23,127,-305,2,16384,0,-306,2,964,SUCCESS
    7,2021-01-06 09:18:17,28.004,0x0016,0x0004,100,100,23,23,25096,-2317,-2316,35.2,1,65535,7,-726,7.0,0,1,28800,1709,0xF8E7,0x0217,0x0400,12,0,16081,23,261,23,131,-302,2,16384,0,-303,2,918,SUCCESS
    

  • Hi Jeffrey,

    The .gg looks ok. There is no alert reset command, the alert pin is asserted by driving low. It will be asserted until the flags are cleared.

    Best regards,

  • Then why is the FC flag not triggering the Alert pint? THat's what the TRM says it should do.  Again - I've configured the Alert pin to assert on several events, including FC. But when the FC flag is raised, no interrupt occurs. What is the reason for this?

  • Hi Jeffrey,

    I will let our FW team know about this issue, this issue was meant to be resolved with G1 version of device.

    Thanks,