This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25710: Alternatives

Part Number: BQ25710
Other Parts Discussed in Thread: BQ25790

Hi,

I'm looking to add an internal charger to my design to interface a battery pack purchased from a third party.

The BQ25710 could do but it has many unwanted features like SMBus and power path; I already have an external power path controller.

Do you have something that comes to mind?

The high switching frequency is very important (> 1MHz).

Thank you

Battery pack specs : 

Cells configuration: 4S2P

Type of chemistry : typical 18650 Li-ions

Gauge : BQ40Z50R1

Pack voltage : 9Vdc to 18Vdc

I'm looking for a charger with those specs :

Charger switching frequency > 1MHz (2-3MHz would be ideal).

Vin (charger) = 12Vdc (fixed)

Charging method : CC-CV

Type : Standalone (no host)

Power Path : Not needed. If there is, I will bypass.