This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM76202-Q1: resistor for Mode selection

Part Number: LM76202-Q1

Hi team,

My customer has question about mode selection.

Datasheet said adding 402k ohm resistor is needed when you choose latched off option.

But they would like to use other resistor value like 390k Ohm. 

I think the IC observe voltage of mode pin, so if the resistor is smaller or larger than 402 kOhm a little( for example , it still work as latched off mode.

Is my understanding correct?

or they must use 402k ohm resistor?

best regards,

Takuya