This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24005: BQ24005/5/6 User Guide (SLUU110A) Table 1-1 is correct?

Part Number: BQ24005

BQ24005/5/6 User Guide (SLUU110A)

page 1-2, Table 1–1.Performance Specification Summary (Two Cell)

Input dc voltage, VDC
Min = 9.1
Typ = 9.5
Max = †VI, for a 2-cell, should not exceed 9.1 VDC for the 1-A charge rate and 10.6 V for the 0.5-A charge rate.

"should not exceed 9.1 VDC for the 1-A charge"
Is 9.1 VDC correct in the phrase?
Isn't it 10.1 VDC?