This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Survey 12V@65A 800W hot-swap solution

Other Parts Discussed in Thread: LM5069

Hi TI,

There is a design requirement for input protection. The functions I need include OCP, Soft start, OVP, UVP, PG, FAULT. Can you recommend it? 

Originally, I tried to use LM5069, but I found that the value calculated by Current limit (Rsns) can't choose such a small resistance value, or can you suggest me a suitable way? Thanks.

Input conditions: 12V, 65A (Total 800W)

BR,

Delun