Hi
As shown in the figure below, if my requirement is Ibus=1.5A and Ibat=1A rechargeable battery, can I set the following? Thank you 1. Set 1.5A in IINDPM 2. Set 1A in ICHG The application after this setting is as follows, please help to confirm that this is correct? 1. When Isys requires 0.5A, the 1.5A of Ibus is divided into two channels (Isys=0.5A for Loader, Ibat=1A for charging) 2. When Isys requires 1.5A, so 1.5A of Ibus is given to Isys, and Ibat=0A does not charge 3. When Isys requires 2.5A, all 1.5A of Ibus is used for Isys plus Ibat=1A, so Isys has 2.5A for Loader 4. Will ICHG be set to 1A, which will restrict the Isys current limit to only 1A output to the Loader? 5. Does Isys have a current limit that can be set?