Other Parts Discussed in Thread: BQ24297
it is not clear from BQ24295 datasheet if the Q1 turns on during boost (OTG) operation. the datasheet shows a phone/tablet connected to PMID. Does the BQ24295 provide 5V on the VBUS when OTG mode is enabled? in the other words, do I need any other connections/components to provide +5V in OTG/boost mode on the same USB connector as I use for battery charging in charge mode?
Thanks!
Yuli