This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2595: bidirectional operation

Part Number: TPS2595

Hi team,

My customer is looking for an eFuse which support bidirectional operation between Vin and Vout. I believe TPS2595 can support customer's requirement.

  • Condition

Vin range : 5V to 10V

Forward current(Vin to Vout) : 0.5A to 2A

Reverse current(Vout to Vin) : 1A to 3A

  • The customer expect following cases.

Case.1 : From the state of VIN < VOUT, turn EN to H(Active) to supply power from VOUT to VIN

Case.2 : From the state of VIN > VOUT, turn EN to H(Active) and supply power from VIN to VOUT, then state is changed to VIN < VOUT and supply power from VOUT to VIN

  • Questions from customer

If the TPS2595 can support Case.1, are the electrical characteristics applied in the Case.1 as well?  Could you also tell me the workable protection function in that case?

The customer's desired protection function is as follows.

The overcurrent protection function does not work in the reverse direction (VOUT-->VIN).
Thermal shutdown works.

Regards,

Yamaguchi