Part Number: TPS53659
Other Parts Discussed in Thread: TPS53681
Hi,
For TPS53659/tps53681, when phase num is larger than 3, is there any special requirement to power stages’ placement?
Can we put the phase 1 power stage between phase 3 and phase 2? The connection is phase1 stage connect to controller PWM1 pin, phase 2 connect to PWM2, and so on.
And is there anything to pay attention if the order is: phase 3->phase 4->phase 1->phase 2, from the left side to the right side in the layout design?(connection is the same as above)
Thanks.
BR
Mason