hi,
from web page of TLV740p, the operating temperature is up to 125C.
Operating temperature range (C)-40 to 125
but the datasheet is recommend to 85C.
can I know which one is correct?
if 85C is correct, for sot23-5 package, the max ambient temperature is -26.69C for 5Vin, 3,3Vout. Is this correct?
85-216*(5V-3.3V)*0.3=-26.69C
BR,
frank