Part Number: TPS1H200EVM
Hello team,
my customer tested the high side switch at 2.5A and it failed. The application is for a BA board. The set up for the 2.5A test was The measurements were performed with a an input voltage of 26.5V, a capacitive load of 470uF and a resistive load to get a load current of 2.5A.
The mentioned device has although passed the 0.4A which the customer would like to test with lower cost devices too.
The current limits were set to 0.74A for the 0.4A application (2700R) and 2.94A for the 2.5A application (680R) and a 330nF cap was connected on the delay pin.
Now in our portfolio we have TPS1H100 and the TPS1H00 devices; do you think these could be more suitable for such testing?
Do you feel the 2.5A test was performed well with the TPS1H200 device?
Thank you for your support.
Best regards,
Adrian