IN (pin #1, supply voltage) is 4.2V in normal conditions
VOUT is set at 3.3V
VIN_OK is set at 3.52V, through the 4 resistors bridge on VRDIV, VIN_OK_SET, VOUT_SET, VON_OK_SET.
Question: could I tie VIN_OK to EN2 -- as shown below -- in order to disable the Buck Converter of the TPS62736 as soon as the VIN voltage, provided by the LiPo battery, falls under 3.52V?
The goal is to preserve the battery life from discharging too much.
Note: the down-stream components are protected against unattended power-off.
Thanks for confirming.