Other Parts Discussed in Thread: TL431
Hi,
I am trying to design AC to DC converter with flyback topology. With input RMS voltage =240V, ouput 24V, 2A. I have used web bench power supply to design this circuit. I have simulated the circuit in TINA but I am not getting desired ouptut. I would like to know the following :
- Web bench has showed this component (LM5021) has capabilities to operate with 240 to 340VPeak to peak. My doubt is in the datasheet of LM5021 the maximum input voltage for VIN is 30V. Does this component has the capabilities to convert VRMS 240 to 24V ? If not this component can you recommend some other component which has tina spice model.
- I would like to know why am I not getting desired output when I have designed the circuit similar to web bench power supply. Is something wrong with Web bench or it is the issue with TINA or my circuit designing? I have used non linear secondary output transformer and editted the total number of windings to suit the requirement. Please let me know what are the changes I will have to make in this circuit to get the desired ouput.
- I have attached my TINA file, WEb bench power supply pdf. 8081.WBDesign40.pdfLM5021.TSC