Other Parts Discussed in Thread: LP5030
Hello,
My questions are in regards to the chip enable (pin 43) of the LP5030/6.
- When disabled via pin 43, does the I2C bus still work?
- When disabled via pin 43, is the firmware still running inside the chip?
- When pin 43 is moved from disable-to-enable, will this impact any of the I2C registers?
- Figure 8.4 would suggest that the device always goes through an initialization sequence and all registers are reset. Please confirm.
- Are there any concerns at startup if pin 43 is high/low?\
Don